This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63020做LED驱动出现的问题

Other Parts Discussed in Thread: TPS63020

TI工程师:

                你们好!我在使用TPS63020做LED驱动时出现一个问题:当我的输入电压为4.2--4.4V,3.7A,输出电压为3.6---3.9V,2.6A时,TPS63020的工作模式却是升压,这个比例是我整批货的比例的6%。由于输入电压比输出电压高,工作在升压模式,所以效率非常低,只有70%。我们将处于降压模式的驱动模组的IC拆下换到升压模式的模组上,发现之前升压的模组也变更为降压了。

                请问TPS63020决定工作模式是否只是根据输入输出电压在内部比较器的比较决定升降压?并且这个输入与输出比较的压差是否必须达到一定的阀值才会进行切换?

                并且我在启动时发现输出会现有一个脉冲,然后才会有输出电压?请问,问题出在那?

  • 亲;这个IC的能力是2A;2.6A是截流保护了。因电流超标;效率自然高不起来。建议用带恒流功能的LED驱动IC做驱动;通用IC并不适合;除非增加稳流电路。

  • 亲;请先看规格书,规格书说在降压模式下能输出3A的电流?截流保护,从何说起?

    我想说的是,为什么TPS63020的IC再相同输入电压相同输出电压的情况下,为什么有的进入升降压混合模式,有的进入完全的升压模式?效率低并不是截流保护,因为我监测到L2脚的波形是完整的方波,未出现杂乱的波形。