This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

請問LM317 動作 溫度約75度C時 適合用SMD(R-PDSO-G4)嗎?

Other Parts Discussed in Thread: LM317

現在用二顆LM317設計電池定電壓、定電流的充電電路,

輸入電壓為24V經過LM317降為13.5V、0.25A對電池充電,在充電過程中,LM317會發熱到75度C左右,請問若我用R-PDSO-G4這個包裝LAYOUT時,IC散熱的地方在PCB板上用小面積鋪錫的方法散熱,不知是否可行?

謝謝!

  • 你的这个充电应用,虽然充电电流很小,但是输入输出电压差非常大,这使得你的效率只有56%,同时也导致你现在的发热严重的现象,我建议你采用开关模式的充电器,它会使得效率得到大幅的提高,避免了发热的问题,同时充电的效率也大大的提高了,若您感兴趣,请您将您的电芯化学类型 和串并联结构,以及是否需要路径管理(终端客户在实际应用时,是否会在充电器插入的时候同时使用负载,即需要充电器一边充电,同时也要给负载供电)等相关项目信息发上来以便为你选择合适的解决方案。

  • this device is compliance with Jedec 020D

  • 每颗LM317损耗(24-13.5)×0.25/2=1.31W,SOT223的QJC=30.6C/W, 芯片内部与外表面的温差为40度,如果目前测得稳定时的温度是75度,芯片内部温度为115度, 允许最高温度为150度,方案可行。