Other Parts Discussed in Thread: TPS62020, TPS63020
我们在使用该芯片做电源管理芯片,输入电压是2.7伏-5伏,输出是1.2伏 电流2安培、2.5伏 2安培、3.3伏 2安培、5伏 2安培。供4路不同的电压输出。在我们的测试过程中,我们发现,空载的时候没有问题,轻载的时候也没有问题,但是当输出稍大一点的负载,该芯片的输出电压就掉下来了,实际输出电流在1A左右的时候,我们的电感用过4.7、3.3、2.2 、1.5 (uH),问题还是不能解决,现在我们用TI的TPS63020EVM_487 DEMO板来测试,还是有这个问题,该板输出3.28伏(空载),然后我们加2.4欧姆的电阻到输出端,这个时候输出电压掉到了2.04伏,我们接1.5欧姆的电阻,输出电压也是掉的很厉害,我们又该变了DEMO板的输出电压,调到1.18伏到1.22伏这个范围,这个时候,该板的空载电压是浮动的,在上面那两个电压上跳来跳去,我们给它的输出加一个1欧姆的电阻负载,发现这个时候输出电压掉到了0.98伏,我们想知道该芯片是否真的和它的说明书上写的一样? 还有,我们要如何解决这个问题? 在测试过程中,我们使用的是直流稳压电源,电压一般设置在3.3伏左右。谢谢!