This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教,双电池串联方案,BQ24133无法充电

Other Parts Discussed in Thread: BQ24133

请教TI工程师,板子使用BQ24133做为充电方案,电池为双锂电池串联,正常电压7.4V,充满8.4V。充电源为升压IC从5V升到9V。升压电路工作正常,电流大于1A。

目前问题是插入USB充电时,从电源计上测试的电流只有150mA左右,包括升压部分。升压电流大概消耗50-70mA。当前电压点为7.1V左右,一直维持这个电压,无法继续往上充电。

各个电压点情况:

VREF: 3.3V 正常。

AVCC: 9.2V

TS: 2.04V

TTC:1.23V

ISET:0.205V

ACSET:0.302V

REGN:6.0V

OVPSET:0.84V

CELL:悬浮

STAT: LOW, 充电和不充电都是

电路图如下: