This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求教如何通过MSP430单片机IO口控制电源通断,以及FET管选型?!!!



想通过MSP430实现对其他设备电源通断控制,由于应用环境为核磁环境,不能使用继电器。电压为24V,电流设计指标1A。

1)开始考虑过通过IO控制具有使能控制的电源芯片,实现外部设备电源的通断控制,觉得有点大材小用,而且器件工作需要一定的压差,所以就没再考虑这个实现途径。

2)如果采用模拟开关控制,这么大的电流恐怕器件也该烧坏了吧?

3)采用达林顿管驱动继电器实现电源通断控制,如前所述,应用环境不允许。

我个人觉得也就只能通过晶体管或者FET进行电源通断控制了,开关电源变换器内部不就是这个道理吗,小弟对于模拟电路研究不够深入,小白一个,

请TI的专家和各位学界牛人帮忙  器件选型,并对430单片机IO口和FET(或晶体管)之间的接口电路设计进行指点。

多谢!!!