如题,输入15-24v 输出30v,效率要达到95%,可以用什么芯片,感谢各位大神指点迷津
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
选择TPS43060这样的同步升压芯片,注意一下电感MOS的选择,做得好满载是可以达到95%以上的的效率的。
你好,
webench 跑一下。
https://webench.ti.com/webench5/power/webench5.cgi?VinMin=15&VinMax=24&O1V=30&O1I=2&base_pn=TPS43060&AppType=None&op_TA=30&lang_chosen=zh_CN&origin=pf_panel&optfactor=3&action=simulate
Hi Chelsea
你好,是输入10V,输出25.4V/3.5A 电流测试,在25度环境下,温度都达到了110度
你好,
功率确实比较大,设计中最好选用小rdson和小热阻的mos,增大板子面积和铜厚,实在不行加额外散热器
要提高效率,需要区分开关损耗和导通损耗谁是主要因素,另外电感的DCR是否足够小。如果开关损耗是主要因素,选择Rds更小的MOS,未必会带来效率的提升。建议做个分析后,再做相应的改进,否则很难给出准确到位的建议。