请问标示4949 21-1是不是LM5021MM-1这颗IC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
负载。我是用电子负载。CC模式下1A,2A.3A都测试。在0.8A下就是轻载这样就工作在调频下。芯片应该没问题哈我换了家代理也一样的。这料是不是很难布线?谢谢你。
对的这个问题已经解决了,是板子走线的问题,谢谢各位了,现在调试有新问题了,现在我重新布了板子,没有干扰了,工作频率正常了,能设定。就我现在的设计参数,85-265V输入电压,输出19V,3.3A。变压器初级24T,次级5T,反馈5T。骨架RM8.电感量85UH.我调试在150K开关频率时工作高低压输入正常工作。但我频率升高到270K时,在低压100V时变压器很大叫声。这时我只有改CS脚上的检流电阻变大,150K时是8个1R并,270K时7个1R电阻并联,这样变压器叫声会有改变,一定的变小了声音。就此我想请教下你就变压器在低压100V高频叫声的问题。恩在270K负载只工作在2.8A以下就没有叫声的100V。到了3A就叫。。有人知道不??