This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335程序烧写到FLASH中,每次上电之后必须手动复位才能正常工作,请问这是什么原因?

TMS320F28335程序烧写到FLASH中,每次上电之后必须手动复位才能正常工作,但是在RAM中运行时不需要手动复位。

复位电路如下:

dsp 1.9V和3.3V电源的上电时序如下,通道1是1.9V,通道2是3.3V:

XRS端上电瞬间电压波形如下,通道1是XRS端电压,通道2是3.3V电源电压:

XRS的低电平时间确实是满足复位要求的,但是为什么程序烧写到FLASH中之后,每次上电之后必须手动复位才能正常工作?求指导,谢谢!