1.出货的时候满充容量和剩余容量都是正确的,EDV都是计算好的,没有问题,参数都是正常的;
2.客户使用50-60个循环退货回来,剩余容量和满充容量都变成300多mAH了,在客户电脑上使用的情况就是充电快,放电也快;
3.不良比率是千分之4左右;
4.客户电脑放电最大电流不超过2A,但是开机的时候有1.5mA的静态电流.
5.不良电池,重新写入正确的GG文件,重新老化,容量还是3900-4000mAh,电芯没有问题.
请教出现这种问题的原因是什么呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.出货的时候满充容量和剩余容量都是正确的,EDV都是计算好的,没有问题,参数都是正常的;
2.客户使用50-60个循环退货回来,剩余容量和满充容量都变成300多mAH了,在客户电脑上使用的情况就是充电快,放电也快;
3.不良比率是千分之4左右;
4.客户电脑放电最大电流不超过2A,但是开机的时候有1.5mA的静态电流.
5.不良电池,重新写入正确的GG文件,重新老化,容量还是3900-4000mAh,电芯没有问题.
请教出现这种问题的原因是什么呢?
电池有在-53度的低温下放过电么?
Lifetime Max Temp = 82.2
Lifetime Min Temp = -53.8
另外有一些配置参数对不上,需要确认下是不是客户有修改过。