This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25119和LM25117问题

Other Parts Discussed in Thread: LM25119, LM25117

大家好!

我使用webench做了lm25119的电源,输入15V,输出7.5V,输出功率20A,加负载时,当负载加到约15A时,整个电路系统似乎进入保护状态,反复启动不能稳定输出。整个电路的哼声听起来也是如此,沙沙沙反复响,温度倒是没有明显升温。

UVLO电压正常,增加软启动时间没有明显效果,短路电流测量电阻没有明显效果,增加自举电容没有明显效果,麻烦给个调试思路。

另外,同样使用LM25117做输入15V,输出12V,12A的电源,问题一致,麻烦提供调试思路,

谢谢!