This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:环境温度与结温的关系

Other Parts Discussed in Thread: UC2844

我非常不明白环境温度与结温的关系。

有三个问题想问一下,都是相关的。

1、我们目前在使用UC2844,供电电压为24V。在环境温度31℃条件下,其表面温度为74℃。我们实际最高的环境温度为60℃,在此条件下,UC2844壳体温度估计为103℃,不知道芯片是否能正常工作?(我们使用的Fluke的Ti10热成像仪来测量的,这个看到的温度是结温Tj还是壳体温度Tc?)
2、你们datasheet的测试条件中说的是“–40°C≤TA≤85°C for the UC284X”“TA = TJ”,也就是说“UC2844 结温Tj在-40度至85度范围内”符合你们的测试结果。是这样理解吗?
3、但你们芯片的最大结温应该是150℃吧,如果以UC2844为例,在Tj=85~150℃的时候,芯片可以不会损坏,但其特性不会同“ELECTRICAL CHARACTERISTICS”中列的一致,这样理解吗?

  • 亲;电路板上还有其它发热东西吗?按理;你的IC不该如此热。60C下;结温也不会达到103C。

    关于用红外测温。由于你用的2844是黑色塑封,是黑体,不能准确测量结温;甚至没太大参考价值。建议用其它方式获得结温。

  • UC2844附近没有其他热源。 供电电压24V,UC2844工作电流12mA,热阻Rja=178℃/W,温升:51.264℃(24V*0.012A*178℃/W)。所以理论上 60℃下,温度为111℃。

    我是觉得:

    UC2844应该只有Tj=-40~85℃的时候 能按datasheet中工作。 在Tj=85~150℃,芯片不会损坏,但性能无法保证。