This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR38020: 使用WEBENCH的设计1.5A能力电路,实际负载能不能满足要求

Part Number: LMR38020


你好:

  使用以下电路,开关频率7300KHz,电感22uH,输入48V,输出12V/1.5A。

负载为1.3A时稳定工作,负载到1.4A时就会出现电压在8V与12V跳变的情况,类似于过流保护的样子。

调整RT电阻阻值调整开关频率,开关频率增大到1MHz时,稳定的负载电流最大只能1A;

调整到如下电路,与datasheet中基本一致,开关频率400KHz,电感33uH,输入48V,输出12V/2A。稳定的负载电流最大只能1.9A,增大到2A就会出现之前的现象。

在稳定输出的情况下,测试12V输出纹波电压只有30mV,看起来很正常,但是稍微增大负载电流就会出现异常。

请问下这种现象是否正常,会是什么原因导致的。