This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

有一个7串700mAh的锂电池组,客户需要个低电压24.7V低电压报警输出



因为是锂电池总电压(21~29V)自身供电,所以希望此电路功耗非常低,希望是uA级
电压低于24.7V,输出低电压输出L(0V),电压高于24.7V,输出H电平(2.4~4.2V)