This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24401: EARLY STOP FAST CHARGE

Part Number: BQ24401


HELLO,

Vin=28.5V, NIMH  cell=20  1.2V/cell

R=75K,C=220nF, MTO=9.88h

In fact,about 4hours later, LED is off, fast charge is stopping .

Why?

Thanks a lot.