This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28711: VS引脚外部电路

Part Number: UCC28711
Other Parts Discussed in Thread: TIDA-00173,

看到这篇帖子的工程师,您好:

我参考了TIDA-00173参考手册,在根据UCC28711D这款芯片进行100~900V反激变换器的设计时遇到如下问题:

根据UCC28711芯片数据手册,VFB辅助绕组电压波形如下:

芯片内部(VS引脚)结构图如下:

根据TIDA-00173参考手册,VS引脚外部电路图如下:

一、当VFB引脚电压为负时,VS引脚内部MOSFET导通,有电流经过R27和D18:

这里我有几个问题:

1. Ivsls的电流从何而来?

因为我不知道LINE SENSE模块的内部图,而电压是施加在MOSFET栅极的,所以我不是很确定Ivsls的电流从何而来;但是根据数据手册,R27的确定公式如下:

 ,所以我只能假设电压为负时,电压主要施加在R27上。

2.D18的反向耐压为何设置为600V?

这个裕量是否过于大了。我个人这里用一个200V反向耐压的二极管就够了,毕竟辅助绕组的电压变化都没有600V。

3.我的最高电压为900V,原边绕组和辅助绕组比值为6,那么辅助绕组最高有150V的负电压,这会导致VS引脚超过它的一个最大1.2V的限值。

参考其他帖子,我打算用如下形式来进行芯片的保护:

 ,但是我这里不知道限流电阻该怎么选取,图中的D6为什么没有限流电阻?难道是R7?但是R7会对采样有影响,我该怎么做?

二、当辅助绕组电压为正时,电压主要施加在R24,R27,R26。这里放置一个R24主要原因是否是可以通过只调节R24将VS的电压在采样时调节到4.05V?