This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756: charge and discharge for supercap

Part Number: BQ25756


我现在想给一个超级电容制作充电器,要求能充电也能放电,充电时先恒流充电然后恒压充电,放电时,恒流放电。超级电容电压范围为2.5-4.2V。要求恒流充放电的电流为38A 。请问有没有相应的芯片?此外,我看了BQ25756,能够双向运行,但是这个芯片反向运行放电时,要求最低的电容电压为3V,请问该怎么处理?

BQ25756对输出电流和电压的控制是开环控制的么,没有找到可以设置PI参数的方法,
MOSFET的占空比是怎么调节的呢?请问
是不是设置了最大的充电电流Ichg后,输出就按照这个
Ichg运行?Rbat_sns电阻采样得到的电流是为了保护,而并未应用于控制MOSFET的占空比?

I am now planning to design a charger for a supercapacitor, which should support both charging and discharging. During charging, it should start with constant current charging and then switch to constant voltage charging. During discharging, it should operate in constant current mode until the lower voltage. The voltage range of the supercapacitor is 2.5V–4.2V, and the required constant current for both charging and discharging is 38A. Could you recommend any suitable chips for this purpose?

Additionally, I looked into the BQ25756, which supports bidirectional operation. However, during reverse operation (discharging), this chip requires the minimum capacitor voltage to be 3V. How can this issue be addressed?besides, the maximum charge and discharge current is 20A. is there any ways to change it?

Is the output current and voltage of BQ25756 open-loop controlled? I have not found a way to set the PI parameters. How is the duty cycle of the MOSFET adjusted? Is it true that after setting the maximum charging current Ichg, the output will run according to this Ichg? The current sampled by the Rbat_sns resistor is for protection, but not used to control the duty cycle of the MOSFET?

  • 您好

    我们会尽快为您调查,请等待我们的回复。

  • 您好

    感谢您在这方面与我们合作。 您能告诉我系统的输入电压和充电电流吗?

    您说:
    如何解决此问题?此外,最大充电和放电电流为20A 有没有办法改变它?
    此问题无法解决。 无法更改充电和放电电流。

    说:
    BQ25756的输出电流和电压是否受过开环控制? 我没有找到设置PI参数的方法
    BQ25756具有所有内部补偿。

    说:
    MOSFET的占空比如何调整?
    占空比由输入电压,输出电压和充电电流调节。

    说:
    设置最大充电电流Ichg后,输出是否将根据此Ichg运行?
    是的,这是真的。 BQ25756将为快速充电阶段提供恒定电流源,为锥形充电阶段提供恒定电压。

    说:
    Rbat_SnS电阻器采样的电流用于保护,但不用于控制MOSFET的占空比?
    我不太确定你所说的是什么意思。 Rbat_SnS电阻器用于控制快速充电电流。 Rbat_SnS还控制正常电池的端接电流。

    您可能已经看到过这一点,但这里是此部分的常见问题解答,仅供参考。

    e2e.ti.com/.../faq-bq2575x-central-faq-page

  • 好的,谢谢。系统输入电压,暂时准备使用20V的系统输入电压。超级电容的充电电流和放电电流都是38A。既然不能更改芯片的最大的可控充电电流20A,那我就准备采用两路并联充放电了。设置最大充电电流Ichg后,BQ25756将为快速充电阶段提供恒定电流源,为锥形充电阶段提供恒定电压。请问,这个快速充电阶段的电流源的电流值是等于已经设置的这个最大充电电流Ichg么?此外,放电时的电流能控制为恒流放电么

  • 您好

    您说:
    在此快速充电阶段中的电流源的当前值是否等于已设置的最大充电电流Ichg?
    是的,这是正确的。 ICHG电流由硬件ICHG设置或ICHG寄存器选择。 IC将选择ICHG的最小值。

    您说:
    此外,放电时的电流是否可以控制为恒定电流放电
    是的,IAC_REV位将限制放电电流。

    您说:
    由于不可能改变芯片的最大受控充电电流20A,我准备好使用两个并联充电和放电。
    这将奏效。

    我还有一个关于该系统的建议。 随着电容器电压下降,BQ25756只能在反向模式下工作,直至大约2.5V。 如果将电容器串联放置,电压将增加一倍,电容将减少一半。 电容器中的功率方程为0.5*C*V2,因此这将使电容器中的可用能量增加一倍。 此外,BQ25756将能够在更大的电容器电压范围内工作。

    如有其他问题,请重新发帖咨询。

  • 好的,非常感谢。
    我想再请问一下,在反向的放电模式下,此时Vbat为系统的输入电压源,Vvac为系统的输出母线电压,反向放电的终止条件是什么,什么时候终止放电,是Vbat下降到3V以下吗?手册中有一句:“When VVAC falls below the undervoltage threshold (programmable via SYSREV_UV register bit), the device stops switching, clears the EN_REV bit, and exits Reverse mode. ”但是这是欠压保护以终止反向模式,而且是VVAC与SYSREV_UV比较然后触发系统反向模式下的欠压保护,系统跳出反向模式。在正常的反向放电模式下,VVAC如果一直在系统正常运行范围内,如何终止放电。 
    此外,两个BQ25756并联,需不需要采取均流措施?

  • 如有其他问题,请重新发帖咨询.

  • IBAT和ICHG是不是相等的?

  • 如有其他问题,请重新发帖咨询.