Hello Ti's expert team,
我们在使用BQ25606进行单节锂电池充电管理设计,我们目前遇到了问题,BQ25606不能按预设定的电流对电池进行充电,下面附上我们的设计图纸及调试过程,请帮忙提供解决思路,谢谢!
1. 电池组,3.7V/6000mAh,内置10K B-3435 NTC,连接到所附图纸的Bat_NTC网络;
2.OTG pin已修改为下拉到GND;
3. D+ D-已修改为悬空;
4. 电池组先做预处理放电至3V,然后在VBUS处加载5V/6A的直流电源,BQ25606未能能对电池组进行稳定输出充电,直流电源显示电流在0与0.5A(近似值)之间跳动;
5. 将D+/D-短接,现象相同;
6. 将D-接GND或+2.8V,现象相同;
7. 将D+接+2.8V,现象相同;
8. 将D+接GND,直流电源显示电流稳定在0.47A。
请问,如何才能将充电电流调整到我们预设的3A?