你好,
我在使用TPS92682的CC模式进行外部PWM调光时,LED会闪烁,设置参照手册8.2.8 Programming Example for Two-Channel CC Mode进行设置,测量后发现,在PWM脚处于高电平时,GATE脚的输出呈现不稳定状态,有时候会在PWM变高之后马上输出高电平,有时候会延迟一段时间之后变高,这样当PWM的频率在5KHz,占空比小于10%时,LED的亮灭会很没有规律,请问是设置的问题吗?
你好,
我在使用TPS92682的CC模式进行外部PWM调光时,LED会闪烁,设置参照手册8.2.8 Programming Example for Two-Channel CC Mode进行设置,测量后发现,在PWM脚处于高电平时,GATE脚的输出呈现不稳定状态,有时候会在PWM变高之后马上输出高电平,有时候会延迟一段时间之后变高,这样当PWM的频率在5KHz,占空比小于10%时,LED的亮灭会很没有规律,请问是设置的问题吗?
您好
首先,你提到GATE脚的输出在PWM脚处于高电平时呈现不稳定状态,这很可能是PWM信号的频率和占空比设置的问题。TPS92682在PWM频率较高且占空比很小时,可能会出现GATE脚输出不稳定的情况。你可以试试调整PWM信号的频率和占空比,看看是否能改善这个问题。
另外,你也可以检查一下TPS92682的内部参数设置,比如软启动时间和电流限制等。这些参数的设置可能会影响到GATE脚的输出稳定性。你可以参考手册中的相关章节,适当调整这些参数,看看是否能解决问题。
还有啊,别忘了检查你使用的外部PWM信号源是否稳定,以及是否与TPS92682的PWM输入脚兼容。有时候,外部信号源的问题也会导致GATE脚输出不稳定。
您好
感谢您的信任
开发板的电气数据是在理想条件下测试所得,且官方给出的典型值是400KHZ,在您设计应用的过程是中请您结合您实际情况来进行匹配。
https://www.ti.com/lit/ds/symlink/tps92682-q1.pdf
具体操作请参考datasheet第24页有相关说明资料。