This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756: Battery Management Studio显示进入快充状态,实际BQ25756没有进入充电状态

Part Number: BQ25756


工作条件:1、PV外接35V/1.5A电源。

           2、输出端口外接12串电池包,电池包总电压39V

           3、打开上位机,关闭WATCHDOG

           4、使能BQ25756、CE端口为低。LED1/LED3灯亮

           5、芯片24脚RENG电压5v正常

           6、芯片23脚DRV_SUP外加8.35V驱动辅助驱动电源 

           7、开启上位机监控显示 Fast Charge (CC mode)

           6、电源实际没有充电电流(如下图所示)。

           7、示波器检测LODRV1/LODRV2没有输出波形,均为高 电平,电压为8.25V左右。

           上位机显示进入快充状态,实际BQ25756没有进入充电状态,拆除MOS,示波器检测LODRV1/LODRV2波形正常,频率220Khz