This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25173: 发热相当严重,Iset电阻为1K,充电电流较小。

Part Number: BQ25173


BQ25173发热相当严重,Iset电阻为1K,充电电流较小。刚焊接好的电路能用,电容充电到预定电压后停止充电(充电过程发热相当严重,手无法触碰),但后面再使用就出现过热停止充电情况,电容电压只充到0.14V,然后一直这样了。超级电容用的是2.7V/35F。layout 遵循TI的参考设计,热焊盘接地良好,有覆铜。期待回复,谢谢。

Power_SuperCap.pdf

  • 原理图看起来不错,没有看到任何问题。
    BQ25173具有内部热限制,如果芯片温度过高,输出电流会降低。当装置进入热极限且输出电流降低时,ISET引脚的电压将降至1V以下。
    当电容器电压接近0V和5.3V输入时,功耗约为2W。机组可能正在进入低输出电流的热调节。
    有几件事可以尝试:
    1.)减少充电电流,以降低设备的功耗。
    2.)在BQ25173或PCB上添加散热器
    3.)并联BQ25173,以划分功耗。