This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40055: 可以提供灌入电流的LDO或者内置MOS的BUCK芯片

Part Number: TPS40055


hi ,我在ADC的输入信号部分接入了二极管用于输入信号过压时,能够将管脚钳位。目前是将二极管的负极接到3.3V电源,通常这对于电源来说是需要有灌入电流的能力的,这边需要大约50mA,但是我看LDO一般不具有灌入电流的能力,TI是否有相关的LDO支持灌入电流。

由于空间有限,或者有相关的可以提供灌入电流能力的内置MOS的BUCK芯片。

总的来说需要12V转3.3V/2~3A,并且需要有灌入电流能力的解决方案。

TPS40055只是控制器,并不是我最想要的解决方案。