This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2897A: 正激电路的整流MOS/栅极驱动芯片耐压问题

Part Number: UCC2897A
Other Parts Discussed in Thread: PMP9656, UCC27511

Hi  sir:

请问正激电路中变压器副边整流电路的耐压是按照什么选择?

是按照 输入除以变压器匝数比的副边电压选择还是正激电路输出电压选择?

UCC2897A应用手册中提到,QF自驱动耐压是按照副边电压;

PMP9656参考设计中的选型应该是按照输出电压来的,器件耐压达不到副边电压。

  • 看起来您混合使用了PMP9656和EVM。

    EVM SR自驱动是通过将次级变压器绕组直接连接到MOSFET来实现的。 因此,需要检查和计算NPS和输入电压导致的绕组电压范围,以确定Vgs在该范围内是否正常

    来自两个驱动器芯片的PMP9656,Vgs UCC27511与以下稳压VDRV电路偏置,因此与EVM不同。 PMP9656 Vgs来自UCC27511,电压为VDRV,因此只要VRDV保持在6.8V左右,变压器绕组电压就不会影响此设计中的Vgs,即变压器绕组电压需要大于6.8V

  • Hi Eirwen:

    参考PMP9656 UCC27511 IN+是连接到次级变压器绕组的VSEC1/2,IN+的耐压为20V,是否需要确认绕组电压范围对IN 引脚的影响?谢谢!

  • D1和D6钳位输入+至VDRV约6.8V,因此也与绕组电压无关。