Other Parts Discussed in Thread: UCC28951
尊敬的各位电源工程师们,对于ucc28951的一些用法特来请教
PFSB的电压模式应用中,将引脚3与引脚4短接后,从引脚2注入一个电压信号进行开环测试,发现电流波形不正确,且根据规格书的推荐增加了D6与D8这两个二极管,但是在开环测试中这两个二极管非常非常热,这是什么原因导致的呢?
D6与D8两个二极管的主要作用是什么?是用来吸收次级反射过来的电压尖峰吗?
此设计输入是DC280V输出是DC28V,Np:Ns是6:1,输出功率为3.5kw,开关频率为100kHz,红色为全桥输出的电压波形,绿色为全桥输出的电流波形
i