This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28951-Q1: 全桥输出的变压器前级的电流波形有很大的振铃和突变

Part Number: UCC28951-Q1
Other Parts Discussed in Thread: UCC28951

尊敬的各位电源工程师们,对于ucc28951的一些用法特来请教

PFSB的电压模式应用中,将引脚3与引脚4短接后,从引脚2注入一个电压信号进行开环测试,发现电流波形不正确,且根据规格书的推荐增加了D6与D8这两个二极管,但是在开环测试中这两个二极管非常非常热,这是什么原因导致的呢?

D6与D8两个二极管的主要作用是什么?是用来吸收次级反射过来的电压尖峰吗?

此设计输入是DC280V输出是DC28V,Np:Ns是6:1,输出功率为3.5kw,开关频率为100kHz,红色为全桥输出的电压波形,绿色为全桥输出的电流波形

i