Part Number: TPS745-Q1
Hi teams,
The load equipment requires the rise time of the power to be greater than 0.15ms
I would like to inquire about the deviation of rise time for TPS745-Q1 .
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS745-Q1
Hi teams,
The load equipment requires the rise time of the power to be greater than 0.15ms
I would like to inquire about the deviation of rise time for TPS745-Q1 .
A rise time greater than 150us should not be an issue with this device, as the lowest rise time this device is guaranteed for is 200us:

The start-up time defined in the datasheet includes delay time an rise time
The delay time is about 200us from fig 6-36.
In limit condition, Can device guaranteed the lowest rise time of 200us?

Since the start-up time includes delay time and rise time, then yes, we should be able to guarantee the lowest rise time is 200us.