This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122 设计为14-17v输入 24V 输出 电路无输出,电路吱吱吱的叫,实际为16.3v输入 输出15.7V

Other Parts Discussed in Thread: LM5122

您们好,前些天用WEBENCH设计的电源 14-17V 升压到24v,无输出,电路吱吱吱的叫,输入电流400ma左右

用万用表打地(9脚)和 UVLO(6脚),吱吱声减弱,输入电流降为17ma左右,但是仍无法工作

UVLO(6脚) 1.615V
VCC(17脚) 7.64V
SS (7脚) 0.428V
HO (19脚) 15.44V

LO无波形,电压=0v

BST(20脚) 25.74V
SW (18脚) 15.39V
FB (10脚) 0.737V

暂时没有示波器,没办法测量,学生党,折腾了四天了,仍然无效果

MOS管为csd17312

附件中上传有自己的原理图,为实际元器件的测量值,WEBENCH仿真的报告 lm5122的手册   ,csd17312手册

Question.rar