This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54540B: 输出电压缓慢降低的问题

Part Number: TPS54540B


我们使用TPS54540B做了一个12V输入、5V输出的电路,原理图如下。

在实际测试中发现,刚上电时,5V输出是正常的,实际为5.08V左右,但过一段不等的时间(几分钟至24小时)后,这个电压会以肉眼可见的速度逐渐降低,最终降低至0~1.2V左右,致使后级电路失效;我们有8个相同的板子,部分板子可以坚持2、3天以上不出问题,但大部分都有类似的情况。下图为PCB设计,展示的为顶层和底层,中间层均为GND

请各位大神帮忙看看有什么想法吗?