This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5157: LM5157低频时SW点波形问题

Part Number: LM5157


RT电阻=220kΩ,负载电流=0.5A,输入=6V,输出=12V,sw点波形如下

呈现出的波形在MOS关断时出现震荡,增加负载电流或者改变补偿网络也没有作用。而改变RT电阻值后,将频率提高至400kHz和2MHz就没有这个问题,提高输入电压至11V,Sw点波形如下

震荡幅度有着明显降低,输入电压升高到12V,sw点波形如下

震荡幅度更小,占空比也升高到98%。

所以这种震荡是正常的情况吗,如果不正常,是有什么原因引起的这种震荡呢?我需要更改什么部分来改善这种情况。