This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS77301的复位信号问题



我使用TPS77301使用电阻 18K / 30K 组合调压输出实测1.92V 。

当输入电压是2.6~2.99V时,输出电压是1.92V,但是Reset都是低电平的。

当输入电压是3.0V时,输出电压是1.92V,Reset才变高电平。

为什么在输出变压都是1.92V时Reset电平只有在输入电压达到3V时才输出高电平呢?

这和芯片什么参数有关?

我怎样才能在输入电压在2.5V,输出电压1.92V时,Reset输出高电平?

TPS77301是否能做到?如果不能,可否推荐合适的器件?