This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS552892: 1206 MLCC电容啸叫

Part Number: TPS552892

工程师你好,

我们选用TPS552892做demo板,输出电压设定为12V,原理图如下所示,电感为4.7uH,IDC为4.5A。

输入电源:KEITHLEY 228S-32-6,负载为电子负载:IT8511。

下图灰色的为第一版layout布局位置和TI 给的demo板位置一致,但并没有在C4、C5、C16、C17之间打很多过孔。

目前上电带负载时,MLCC电容会出现不明显的啸叫,我尝试调整过FSW和SYNC效果并不明显,且在输入不同电压会有1%的输出电压偏移,偏移时啸叫会有明显变化。MLCC选用10uF/50V/1206

请问是否为过孔偏少导致的还是其他原因导致的?下方PCB是修改加过孔后的图也帮忙看一下是否有问题,谢谢

感谢。