This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI工程师好,有个相关LM5088的应用请教下
1、75V输入,12.6V@10A输出,对于LM5088这些参数都接近max能力值
以上的参数,LM5088能够满足?按我的理解,LM5088的最大输入范围是75V,如果我的工作状态是75V,没有裕度,可以吗?
另外:LM5088的散热在75V输入的情况下是很严重的一个问题,加散热片够吗?还是要加风扇?
TI是否有相关的DEMO可以测试?是否有好的建议
亲;首先,如果额定最高工作电压75C,也无法完全保证一定在任何时候不超,当然;略微超也不一定损坏。从条理上讲;你的做法有风险,建议不要这么做。
其次;CS/CSG对GND的极限值是+-0.3V,这么大电流;要保证这点过电压,对PCB设计者来讲;是非常疯狂的,75V下几乎肯定会超标。
因此;换方案为妙。
LM5088是非同步的方案,肯定不适合这么大功率的应用,推荐LM5116同步方案。
75V肯定不行,散热的话用controller也没问题。你推荐100V的controller来做,比如LM5116或LM5117.