This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5088 设计方案75V输入 12V@10A输出

Other Parts Discussed in Thread: LM5088, LM5116, LM5117

TI工程师好,有个相关LM5088的应用请教下

1、75V输入,12.6V@10A输出,对于LM5088这些参数都接近max能力值

以上的参数,LM5088能够满足?按我的理解,LM5088的最大输入范围是75V,如果我的工作状态是75V,没有裕度,可以吗?

另外:LM5088的散热在75V输入的情况下是很严重的一个问题,加散热片够吗?还是要加风扇?

TI是否有相关的DEMO可以测试?是否有好的建议