This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76200: Direction for use PACKDIV PIN

Part Number: BQ76200

How to understand that the loading current should be less than 500uA, and what will happen if it is greater than 500uA?

  • 感谢您对TI产品的关注!
    关于你的咨询,BQ76200的PACKDIV引脚用于分压器配置,通常用来监测电池组的电压。
    PACKDIV引脚的负载电流应小于500μA,这主要是为了确保准确的电压读取和电路的正常工作。
    如果负载电流超过500μA,可能会发生以下几种情况:

    PACKDIV引脚的设计目标是提供精确的电压控制。
    如果负载电流过大,可能会引起不再处于线性工作区,从而导致测量的电压值不准确。
    过大的负载电流会导致功耗的增加,可能损害芯片的长期可靠性和稳定性。

    谢谢!

  • “可能损害芯片的长期可靠性和稳定性”关于这个是怎么理解

  • 超过推荐规格使用,芯片有损坏风险或者参数不稳定。