This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51200: TPS51200DRCR(TI)给DDR_VTT&VREF 供电 0V6,上电后DDR抽电流超3A导致1V2上电不单调

Part Number: TPS51200


我司最近有个项目DDR供电电压1.2V上电不单调,不单调的原因是DDR_VTT&VREF 0.6V上电后DDR会抽超3A的电流,时间40us左右,超过了1.2V的输出电流(3A)导致DCDC来不及响应

电流正常是1A左右

帮忙看看为什么TI的芯片会导致DDR抽这么大的电流,谢谢~

 

0.6V用了TITPS51200DRCR(TI)

电子料_IC_电源管理类芯片: Power IC,PM,For DDR/DDR2/DDR3/DDR4,2.5~3.3V,3A,VSON-10,TPS51200DRCR(TI),MSL2

 

电源部分原理图:

 

测量了PU3VINSW 、电感电流、Vout,电感电流某一时刻超3A导致不单调,测试波形:

测量了PU3Vout、电感电流和U1M1 0.6V1.2V电感电流在0.6V上电的时候超3A,测试波形:

U1M1换成TPL51200-DF8R(3PEAK),电流正常1A左右,1.2V单调,测试波形: