This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG2100EVM-097: 在使用两个单独的PWM输入来独立控制HI,LI时问题

Part Number: LMG2100EVM-097

当使用两个单独的PWM输入来控制HI,LI时,单输入频率高于5MHZ,SW输出电压有压降,该压降逐渐加大,脉冲群有150KHz左右的频率。

当频率等于5MHz,SW输出电压没有压降,脉冲群有150KHz左右的频率。

当使用1MHz时以上现象均没有。

输出波形如下。以上所有情况均拆除了4.7uH电感。