使用BQ24610,原理图按datasheet上的连接,使用19V对三串锂电池进行充电。目前插入锂电池可以对负载进行供电;使用外接电源也能对负载进行供电。但是不能对锂电池进行充电。datasheet上说,只是插入外接电源时,STAT1 OFF;STAT2 OFF,接上的LED应该灭。但是STAT1不是完全的高电平,导致与STAT1 连接的红色LED仍然亮。与PG端连接的LED是亮的,显示外接电源正常。问题:(1)不能对锂电池充电 (2)直接入外接电源时候,为什么与STAT1相连的LED亮?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用BQ24610,原理图按datasheet上的连接,使用19V对三串锂电池进行充电。目前插入锂电池可以对负载进行供电;使用外接电源也能对负载进行供电。但是不能对锂电池进行充电。datasheet上说,只是插入外接电源时,STAT1 OFF;STAT2 OFF,接上的LED应该灭。但是STAT1不是完全的高电平,导致与STAT1 连接的红色LED仍然亮。与PG端连接的LED是亮的,显示外接电源正常。问题:(1)不能对锂电池充电 (2)直接入外接电源时候,为什么与STAT1相连的LED亮?
谢谢你,但是我还是不能解决这个问题,以下是测量的一些电压值:
(1)使用外接电源19v,无电池,无负载:
PG is 0.11V
STAT2 is 17.36v
STAT1 is 11.5v
Vref is 3.297v
TS is 1.687v
REGN is 6v
VFB is 0.017v
(2)使用外接电源19v,接入锂电池12.2v,无负载
PG is 0.112V
STAT2 is 17.34v
STAT1 is 11.57v
Vref is 3.364v
TS is 1.721v
REGN is 6.12v
VFB is 1.989v
下面是原理图:

希望大师指点一下。