This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于使用BQ24610的问题

Other Parts Discussed in Thread: BQ24610

使用BQ24610,原理图按datasheet上的连接,使用19V对三串锂电池进行充电。目前插入锂电池可以对负载进行供电;使用外接电源也能对负载进行供电。但是不能对锂电池进行充电。datasheet上说,只是插入外接电源时,STAT1 OFF;STAT2 OFF,接上的LED应该灭。但是STAT1不是完全的高电平,导致与STAT1 连接的红色LED仍然亮。与PG端连接的LED是亮的,显示外接电源正常。问题:(1)不能对锂电池充电 (2)直接入外接电源时候,为什么与STAT1相连的LED亮?

  • 樓上所提到的現像應該是動態路徑管理啟動了,查一下你的ISET1電壓設定多少?ACSET電壓設定多少?

    ISET1設定充電電流,ACSET設定電源總輸入電流,當負載電流+充電電流>設定的總輸入電流時IC開始下調充電電流;

    當負載電流≧設定的總輸入電流時關斷充電電流,优先負載電流。

    STAT1/STAT2的邏輯建議再仔細看看規格書,這個充電方案整體效果還不錯。

  • 谢谢您的帮助!也谢谢您关注我们的论坛!

  • 谢谢你,但是我还是不能解决这个问题,以下是测量的一些电压值:

    (1)使用外接电源19v,无电池,无负载:

       PG is 0.11V

     STAT2 is 17.36v

     STAT1 is 11.5v

     Vref is 3.297v

     TS is 1.687v

     REGN is 6v

     VFB is 0.017v

    (2)使用外接电源19v,接入锂电池12.2v,无负载

     PG is 0.112V

     STAT2 is 17.34v

     STAT1 is 11.57v

     Vref is 3.364v

     TS is 1.721v

     REGN is 6.12v

     VFB is 1.989v

    下面是原理图:

     

    希望大师指点一下。