This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28180: 低电压使用

Part Number: UCC28180

我需要设计一款PFC电路,输入为交流15V至19V,输出36V直流,最大电流2.5A,不知道用UCC28180是否可以。我试了用WEBENCH工具来设计电路,但是该工具对于UCC28180芯片,只支持46V,不知道UCC28180是否不可以用于15VAC的低压。我也用了SLUC506计算工具计算了相关参数,但是做出电路后无法完成。请问我该怎么设计。能否有相关参考电路或请相关工程师帮助。谢谢!