This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

用Step-Down芯片TPS54232做了一个负电压电源,芯片很烫,输出电压也不够,什么原因?

Other Parts Discussed in Thread: TPS54160, TPS54232

电路如图,就是把典型的正电压电路的地和输出做了对偶的互换。

对应的正电压电路(已制板验证,电路可以正常工作)如下图:

是哪个地方有问题?

是不是这个芯片不支持这么用?

如果是,求推荐一款可以既可以做正电源又可以做负电压的芯片,输入24V,输出±15V,电流1A以上就可以,频率要尽量高。

谢谢!