Other Parts Discussed in Thread: LM5170
LM5170,预期设置调试为buck模式用于输出12v电压,做了以下步骤调试步骤: 第一步HV_PORT端口用外部恒压源1给定48v直流电压 第二步:VCC和VCCA口是用外部恒压源2提供12v电压,再用12V转10v的LDO(500MA带载能力)给定10v直流电压 第三步:DIR口用外部恒压源3给定5v电压 第四步:EN1 , EN2 , UVLO这三个脚电气连接在一起,用外部恒压源3给定5v电压 上述4个步骤按顺序给完后,测量结果是,输入HV_PORT电压48v, 输出端口LV_PORT端口电压4.3v, VINX脚没有电压 RAMP1 RAMP2也没有震荡斜坡信号,相当于LM5170内部振荡器没有起振,烦请帮忙看下是什么原因