This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5170-Q1: 上电后没有起振

Part Number: LM5170-Q1
Other Parts Discussed in Thread: LM5170

   LM5170,预期设置调试为buck模式用于输出12v电压,做了以下步骤调试步骤:   第一步HV_PORT端口用外部恒压源1给定48v直流电压     第二步:VCC和VCCA口是用外部恒压源2提供12v电压,再用12V转10v的LDO(500MA带载能力)给定10v直流电压          第三步:DIR口用外部恒压源3给定5v电压         第四步:EN1 ,  EN2 , UVLO这三个脚电气连接在一起,用外部恒压源3给定5v电压      上述4个步骤按顺序给完后,测量结果是,输入HV_PORT电压48v,  输出端口LV_PORT端口电压4.3v,  VINX脚没有电压   RAMP1  RAMP2也没有震荡斜坡信号,相当于LM5170内部振荡器没有起振,烦请帮忙看下是什么原因