This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3707: TPS3707看门狗激活方式

Part Number: TPS3707


您好,请教一个关于看门狗的问题:TPS3707或者类似的带看门狗功能的监控芯片,看门狗的激活方式是啥?是否为WDI引脚有电平翻转,比如从“0”到“1”,或者从“1”到“0”?如果看门狗芯片的WDI连接至处理器(DSP或者ARM或者FPGA)的I/O引脚,初次上电后不想立刻激活看门狗,而是想在处理器完成软件加载后,可选择性的激活或者不激活看门狗,应该如何设计该电路?如果处理器在启动配置过程中(大约及时秒)I/O引脚的电平默认为“1”(弱上拉),处理器配置完成,软件运行后该I/O同样赋值为“1”,是不是可以理解为看门狗一直不回被激活?请帮忙梳理并回复,谢谢。

  • 笔误:

    1)“大约及时秒”应为“大约几十秒”

    2)“不回被激活”应为“不会被激活”

  • 您好,   

    如果处理器在启动配置过程中(大约及时秒)I/O引脚的电平默认为“1”(弱上拉),处理器配置完成,软件运行后该I/O同样赋值为“1”,是不是可以理解为看门狗一直不回被激活?

           您这种情况是一直没喂狗,启动完成要几十秒的话,太长了。

            请注意只有TPS3705-xx具有watchdog time,TPS3707没有

           请参考芯片数据手册“8.3.3 Watchdog Timer”,芯片上电工作后 watchdog timer即启动,

           如果WDI在1.6秒内没有电平翻转,则WDO输出。

            Processor Supervisory Circuits with Power-Fail datasheet (Rev. F)

  • 比如系统使用AM335x等处理器,操作系统启动时间就是很长,此时看门狗电路应该如何设计?只能等AM335x的系统起来后再执行喂狗,所以要确保在AM335x启动配置过程中,看门狗不被激活,所以在上电到AM335x配置这段时间,看门狗芯片的WDI应该如何设计才能确保电路正常工作。另外,看门狗确定是上电不需要配置就被激活?还是需要WDI有电平翻转或者固定电平?这点很重要!

  • 您好,

          是的

    请注意只有TPS3705-xx具有watchdog time,TPS3707没有

           请参考芯片数据手册“8.3.3 Watchdog Timer”,芯片上电工作后 watchdog timer即启动,

     

    在上电到AM335x配置这段时间,看门狗芯片的WDI应该如何设计才能确保电路正常工作。

    新问题请重新发帖