This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23758: TPS23758 DC12V供电下输出5V掉电

Part Number: TPS23758
Other Parts Discussed in Thread: , TPS23755

我们使用了TPS23758EVM-080设计了两款产品,使用外部DC 12V电源供电,原理图参考了TPS23758EVM-080。

这两款产品的PCB是一样的,区别在于TPS23758的5V输出端负载不同。A产品12V输入端的功耗在4W以下,B产品12V输入端的功耗会达到5W。

目前A产品已经设计定型,并且有两台样机我们用来长期测试,持续上电运行了超过6个月,并无出现异常。

B产品最近在挂载测试,我们发现B产品的部分样机,会无预见性的出现5V输出端下电的情况,有时候挂机半小时出现,有时候挂机1个小时出现,并且输出端下电出现后,通常会恢复输出几次,然后机器还能运行几分钟,但是最终,5V输出端都会完全关闭,此时12V输入端功耗只有几mA。

请问为啥会存在这种情况?是否可以解决?