This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP38798损坏问题

Other Parts Discussed in Thread: LP38798

各位:
    最近项目中用到LP38798时出现了损坏,12V输入,10V输出的LP38798有比较高的概率;
    附件是原理图的一部分,原理是外部程控电源12V供电,限流1A(正常供电时电流为0.14A),12V输入端有一颗100uF高分子铝电解电容,板子上除了有基本的电源芯片,还有两路 DCDC(见原理图第3页)输入也是12V供电;
    PCBA厂刚拿回来的板子,上电前,测量各电源的输入输出对地阻抗均正常,在程控电源第一次给板子上电的过程中,会出现1A过流保护,电压被拉下来;
    再开关两次程控电源后,程控电源输出稳定12V,电流为0.14A,这时有的板子上的LP38798会出现输出电压为0V的情况,而有些板子LP38798 10V输出全部正常;出问题的片子都在TOP面,在BOTTOM面也有一片38798(U84),是5V转3.3V,这个片子均没有坏的;
    出问题的片子拆下来后,测量片子的6、7脚会导通,而好的片子则是高阻。
    而当将程控电源限流设置到0.3A时,第一次给板子上电,程控电源不会出现过流,而且38798没有坏的。

    之前有四路 DCDC(见原理图第3页)时LP38798没有坏的情况出现;

各位帮忙分析下,万分感谢!

two_channels20151112.pdf