在使用BQ25750为6节4.2V电池(满电为25.2V)充电的过程中,升降压MOS发热十分严重。
输入电压24V,电感感值选用10uH,ICHG通过电阻设置5A充电,FSW_SYNC设置为200kHz开关频率,DRV_SUP使用外置DCDC供电10V。
开启电池充电后,测得实际充电电流为3A左右,示波器测得开关频率200kHz符合设置。
升降压MOS持续升温,在120℃左右稳定,这对于系统来说温度太高了。请问这种情况属于正常情况吗,有什么方法可以解决MOS温度太高的情况。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在使用BQ25750为6节4.2V电池(满电为25.2V)充电的过程中,升降压MOS发热十分严重。
输入电压24V,电感感值选用10uH,ICHG通过电阻设置5A充电,FSW_SYNC设置为200kHz开关频率,DRV_SUP使用外置DCDC供电10V。
开启电池充电后,测得实际充电电流为3A左右,示波器测得开关频率200kHz符合设置。
升降压MOS持续升温,在120℃左右稳定,这对于系统来说温度太高了。请问这种情况属于正常情况吗,有什么方法可以解决MOS温度太高的情况。
我只是在快速了解这个话题。据我所知,初始分压器会将设备置于VAC_DPM。ACUV阈值设置设备的操作窗口。有一个高于ACUV限制的阈值,用于设置VAC_DPM范围,这将限制输入电流。我相信伊森注意到波形表明电路中有一个小电流。
ACUV限值由以下方程式确定:
VVACUVP=1.1(RAC1+RAC2+RAC3)/(RAC2+RAC3)
ACUV_DPM限值由以下方程式确定:
VACUV-DPM=1.21(RAC1+RAC2+RAC3)/(RAC2+rac三)
基于初始电阻分压器,ACUV_DPM限制高于测量的VAC电压,这将使设备进入电压DPM,设备将限制电流。您能否通过第一个电路找到I2C读数以查看VAC_DPM_STAT位的值来验证这一点?