• EV2400

    chakanDIANCHI参数

  • BQ25756EVM: TPS26750EVM與BQ25756EVM配置

    Part Number: BQ25756EVM
    Other Parts Discussed in Thread: TPS26750EVM, EV2400

    您好,

    目前在配置使用TPS26750EVM+BQ25756EVM來進行PD3.1充電測試,

    現在有使用USBCPD_Application_Customization_Tool對TPS26750EVM設定,

    同時在BATTERY CHARGER CONFIGURATION也有針對BQ25756EVM進行設定,

    將USB充電器插入J4時,J7(PPHV…

  • BQ25750EVM: 目前使用BQ25750充电电压不正常问题

    Part Number: BQ25750EVM
    Other Parts Discussed in Thread: BQSTUDIO, EV2400, , BQ25756, BQ25750

    在输入电压开始为11V时,其充电电压为EVM板子默认充电电压22V,在输入电压从11V增加到20V时,其充电电压从22V增加到接近30V.但输入电压达到21V时,其充电电压变为7V左右。设置输入电压大于20V时,其充电电压都小于默认充电电压。使用EV2400在BQStudio上查看芯片寄存器数据都在正常范围,请问这是板子哪方面出来问题了…

  • BQ34Z100: Battery Management Studio 配置 BQ32z100 问题

    Part Number: BQ34Z100
    Other Parts Discussed in Thread: EV2400


    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi Portuguese
    Catalan Hmong Daw Romanian
    Chinese Simplified Hungarian Russian
    Chinese Traditional Indonesian S…
  • BQ27Z746: EV2400与上位机连接断开

    Part Number: BQ27Z746
    Other Parts Discussed in Thread: EV2400, BQSTUDIO, BQ76952

    连接好好的,突然就与BQstudio断开连接了,显示找不到免费的通信适配器,请各位大佬指点一下这是什么原因呢!难道是因为电脑主机供电不足,导致EV2400断开了嘛?

  • BQ25756E: 纯电阻编程时芯片不能正常工作

    Part Number: BQ25756E
    Other Parts Discussed in Thread: EV2400, BQSTUDIO,

    您好!

    我们最近在使用贵公司的BQ25756E芯片进行无线充电应用。由于我们的I2C编程经验较少,因此选用纯电阻编程,电路图参考评估板与datasheet电路如下.。input端即为芯片datasheet中的input,在整体电路的基础上我们在图右上方添加了有驱动芯片的放

    电电路。在目前的初步测试中我们将SCL SDA INT三个与I2C编程相关的接口悬空…

  • BQ76952: BQ76952上电参数无法读取,能读到没串电压,提示CRC error detected in block read from device using l2CCRC communications protocol

    Part Number: BQ76952
    Other Parts Discussed in Thread: EV2400

     BQ76952 无法读取参数,提示CRC error detected in block read from device using l2CCRC communications protocol 

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi Portuguese
    Ca…
  • BQ27427: 为何充电时电量会停止在99%?

    Part Number: BQ27427
    Other Parts Discussed in Thread: EV2400, BQSTUDIO

    如题,我是用EV2400直接连接我的PCB,该PCB上仅有BQ27427一个I2C器件,BQ studio软件可以正常的读取到相关信息,如图所示,电池的相关信息都已经设置,但是充电时一直停止在99%,FC标志无法置位,也无法完成自学习,请问这是什么地方未配置呢?

    4.gg.csv

  • EV2400: 三个指示灯不亮了

    Part Number: EV2400

    EV2400接电脑USB输入,指示灯本来是亮的,现在不亮了,买来半天

  • BQ25756E: 我在使用bqStudio软件时,无法连接到芯片,请问是需要安装某些驱动吗

    Part Number: BQ25756E
    Other Parts Discussed in Thread: BQSTUDIO

    我在使用bqStudio软件时,无法连接到芯片,请问是需要安装某些驱动吗

  • EV2400: 设备管理器无法无设备显示

    Part Number: EV2400

    电脑连接EV2400,设备管理器并没有找到相应设备,但是有刷新,无法正常使用,请问是需要什么固件吗

  • BQ27531-G1: 电量计data-flash参数丢失问题

    Part Number: BQ27531-G1
    Other Parts Discussed in Thread: BQSTUDIO, EV2400, , BQ24192

    我们的设备正在使用bq27531-g1和bq24192方案,并使用bqstudio+EV2400工具,将调试好的.srec文件烧录到电量计芯片中;

    随后,我们在设备不带电池的条件下,进行外部电源通电、断电的测试,一段时间后,发现电量计芯片的data flash的参数丢失,恢复成了默认值。

    请问对芯片断电上电会导致data flash里的参数丢失吗…

  • BQ40Z50-R1: FCC 衰减和电池激活

    Part Number: BQ40Z50-R1
    Other Parts Discussed in Thread: EV2400,

    Hi

    关于客户电池激活和FCC 衰减问题,还请帮忙确认下。谢谢

    1. 我们带PRES使用功能的电池遇到一个问题:电池15天搁置后,进入到ship模式,然后短接电池上的PRES脚到P-,电池使用直流电源8.7V/2A进行充电,电池无法唤醒激活。但是当我们使用EV2400通信盒连接上位机同时对电池进行通信下,可以正常使用直流电源充电激活电池。电池激活后我们使用上位机软件发…

  • BQ27Z746: EV2400

    Part Number: BQ27Z746

    电池连接上上位机  没有任何负载  但是显示有电流放出  这是什么原因呢

  • EV2400: EV2400 no acknowledge from device

    Part Number: EV2400
    Other Parts Discussed in Thread: BQSTUDIO

    您好!

    1. 打开软件后发现EV2400 no acknowledge from device

    2. 也看到过一个提示是operation failed because initial read of all data flash failed

    3. 点击data memory时发现import from file(advanced)显示灰度,无法选择

    烦请指导一下如何解决…

  • BQSTUDIO: bq40z651的相关问题

    Part Number: BQSTUDIO
    Other Parts Discussed in Thread: EV2400

    bq40z651与ev2400如何连接,如何通过bqstudio来检查电池元器件的状态,另外我想请问下初始的key是多少?

  • BQ25756: 无法工作

    Part Number: BQ25756
    Other Parts Discussed in Thread: EV2400,

    您好!

          我们现在有个项目,采用BQ25756RVRR,也有评估板,但现在存在以下问题:

          1. 上电后用EV2400观察,芯片配置,状态正常;

          2. 输入电源25V,驱动电压(外部)10V,都正常;

          3. 但板子无输出,还经常烧坏MOSFET,BQ25756也会损坏。

          请问,这个是什么原因。

          原理图:

          

          PCB layout:

  • BQ25756: BQ25756, BQSTUDIO

    Part Number: BQ25756
    Other Parts Discussed in Thread: BQSTUDIO, EV2400

    BQ25756 支持I2C和standalone配置。请问,如果需要使用I2C配置寄存器,下载安装BQSTUDIO软件,然后USB连接PCB板,配置BQ25756,还需要别的硬件么

  • BQ25756EEVM: BQ25756

    Part Number: BQ25756EEVM
    Other Parts Discussed in Thread: EV2400

    你好,怎样利用Battery Management Studio,来调试MPPT功能

  • BQ25756: Questions about the charging status.

    Part Number: BQ25756
    Other Parts Discussed in Thread: BQSTUDIO, , EV2400

    Excuse me. Based on what information does the current charging status of the charging chip (REG0x21--[2:0]) change automatically? If it is judged according to the current battery…

  • EV2400: 使用bqStudio前面若干次都可以读取所有地址值,操作几次后就部分高位地址无法读取

    Part Number: EV2400

    0x38以下地址仍可以读取,40及以上就全部返回错误

  • BQ34110: 配置BQ34110时,BQ Studio总是提示Pack Voltage correction is beyond allowed range.

    Part Number: BQ34110
    Other Parts Discussed in Thread: EV2400, BQSTUDIO

    用EV2400连接我自己的PCB,去掉了不需要的跳线和电压分压网络,最终电压分压网络如上图。8节磷酸铁锂串连最高电压29.2V,BAT点最高电压899mV。

    目前读取温度电流什么的都没问题,但电压是0。现在正在配置电池参数,按照bq34110EVM-796 Evaluation Module (Rev. A)在BQ Studio里执行了以下步骤:

    0.将D…

  • EV2400: win11上使用bqstudio识别异常

    Part Number: EV2400
    Other Parts Discussed in Thread: BQSTUDIO

    我们已经在多台电脑上出现了EV2400不兼容Win11的情况了,

    已经做过交叉验证,EV2400在win10系统上正常运行,

    在win11上设备能识别到EV2400,但是BqStudio就是识别不到,updater也是识别不到.无论换了什么BqStudio版本都是识别不到.

    论坛上也看到比较多人反馈了,希望官方引起重视...

  • BQ27546-G1: 烧录过程莫名提示错误并且无法再进行通讯

    Part Number: BQ27546-G1
    Other Parts Discussed in Thread: BQSTUDIO, , EV2400

    我司使用的BQ27546-G1的电源芯片,产线上使用锂电池做为电源使用EV2400通讯烧录导出的dffs文件,烧录过程中提示read compare line 40,提示之后bqstudio无法再和电量计进行通讯,出现概率极高。望解答

  • BQ40Z50-R1: BQ40Z0-R1方案的4S

    Part Number: BQ40Z50-R1
    Other Parts Discussed in Thread: EV2400

    TI的专家们好!

           我用BQ40Z0-R1方案的4S电池组,客户用机器对电池进行插拔测试,测试中发现有些电池突然没有了输出,用EV2400也无法进行通讯,对电池的PACK+、PACK- 接个直流电源激活下,通讯又正常了,电池有16V多的电压 这是什么情况?

1 2 3 4 5 »