• UCD3138064: KD_ALPHA_1 setting and PID at DYN setting suggestion

    Part Number: UCD3138064

    I would like to ask KD_ALPHA_1 setting

    KD_ALPHA_1  can set to how big and any suggestion for tuning KD_ALPHA_1 

    and the PID at DYN  suggestion
    use two psu current shearing and doing dyn 0.1us /0.1us 22.5A ~470A slew rate was 5a/us

  • UCD3138: no devices found

    Part Number: UCD3138

    我在使用UCD3138CC64EVM-030测试板卡的时候出现了些问题,我真诚的希望有人能帮我解决他们。

    我的连接如图所示:

    使用Device GUI的Scan Device in ROM出现以下正常情况:

    然后我进行下载,就出现了问题:(在program mode中无DEVIVE_ID回应)

    然后我点击scan for device id出现一下问题

    请问大家能帮帮我解决一下吗,非常感谢。

  • UCD3138: 不能下载固件

    Part Number: UCD3138

    您好,能否提供一下下载链接,不知道为什么我不能下载

  • UCD3138: 使用PMBus master 功能

    Part Number: UCD3138

    Hello,

    We need to communicate with battery by PMBus as a matster. And block read and block write function are needed.

    But I can't find the demo code for reference.

    Where can I find it?

    Thanks!

  • UCD3138_FW_SDK: 能否透過UART來進行檢測與調機動作

    Part Number: UCD3138

    您好,

    FW將會基於BI-DCDC的範例程式進行修改,

    主要想把UART功能加上,透過UART來進行檢測、調整PID或是電壓電流等數據。

    想請教如果要針對UCD3138開啟UART的功能,能有什麼資訊可供參考嗎?

  • UCD3138: Uart与Pin脚的对应配置

    Part Number: UCD3138

    用的40Pin的只有一组uart端口,即为SCI_TX0和SCI_RX0;

    但是对应SCI_TX0为Pin9和P22,SCI_RX0为Pin10和P23

    配置如下

    Uart0Regs.UARTIOCTRLRX.bit.IO_FUNC        = 0x01;      //使能UART引功能  

    Uart0Regs.UARTIOCTRLTX.bit.IO_FUNC       = 0x01;      //使能UART引功能

    Uart0Regs.UARTIOCTRLSCLK.bit…

  • UCD3138CC64EVM-030: 电脑无法安装CCS6.2版本,如何解决ucd3138的匹配问题?

    Part Number: UCD3138CC64EVM-030
    Other Parts Discussed in Thread: UCD3138, FUSION-DIGITAL-POWER-STUDIO

    ucd3138需要安装ccs6.2版本进行编译,但是无法安装,请问有别的可替代版本吗

  • UCD3138: 能否用作电流模COT控制

    Part Number: UCD3138

    请问可以用UCD3138来做一个电流模COT控制的buck变换器吗

  • UCD3138CC64EVM-030: JTAG无法连接

    Part Number: UCD3138CC64EVM-030
    Other Parts Discussed in Thread: UCD3138

    板子:UCD3138CC64EVM-030

    调试探针:XDS110 JTAG 

    环境:Code Composer Studio 11.0.

    问题:按照参考文档《避免 UCD3138 器件锁定》中如何使用JTAG解锁一节的步骤操作(当然我们的目的不是解锁器件,而是想通过JTAG成功连接器件),在Test Connection后,出现error,无法成功使用JTAG…

  • UCD3138: DPWM配置

    Part Number: UCD3138

    请问UCD3138 DPWM模式配置为三角波模式时,开环模式下如何改变占空比?应该设置哪个寄存器?

  • USB-TO-GPIO2: UCD3138最新燒錄軟件2022報錯issue

    Part Number: USB-TO-GPIO2

    兩個問題點如下

    1.现請購的USB-TO-GPIO2更新軟體TI-Digital-Power-Production-Tool-2.0.28不能连续烧录,燒錄完一次更換產品燒需要重啟軟體才能燒錄下一台產品,不重啟軟體就會報錯燒不了(如下圖),使用舊版燒錄器USB-TO-GPIO可以正常连续烧录,無此問題,

    2.安裝TI-Fusion-Digital-Power-Studio-3.0.77無法進入軟體界面,但是使用舊款2006版的燒錄器可以進入軟體界面…

  • USB-TO-GPIO2: UCD3138最新燒錄軟件2022

    Part Number: USB-TO-GPIO2

    兩個問題點如下

    1.现請購的USB-TO-GPIO2更新軟體TI-Digital-Power-Production-Tool-2.0.28不能连续烧录,燒錄完一次更換產品燒需要重啟軟體才能燒錄下一台產品,不重啟軟體就會報錯燒不了(如下圖),使用舊版燒錄器USB-TO-GPIO可以正常连续烧录,無此問題,

    2.安裝TI-Fusion-Digital-Power-Studio-3.0.77無法進入軟體界面,但是使用舊款2006版的燒錄器可以進入軟體界面…

  • UCD3138: 请问这个芯片的软件开发环境是什么? 也是CCS吗?

    Part Number: UCD3138
    Other Parts Discussed in Thread: C2000WARE,

    请问这个芯片的软件开发环境是什么?  也是CCS吗?

  • UCD3138: UCD3138 for full-bridge LLC

    Part Number: UCD3138

    Sir 您好

    目前要使用UCD3138控制 Full bridge LLC,請問有軟件包嗎?

    Thanks,

    Sam

  • UCD3138: UCD3138用户bootloader开发

    Part Number: UCD3138

    有关UCD3138 用户bootloader 开发

    UCD3138中没有找到中断向量表重定位寄存器,因此,想问在设有用户bootloader的环境中,用户app的中断向量表和bootloader的中断向量表如何实现重定位呢?

  • UCD3138: 如何加密程序,防止复制

    Part Number: UCD3138

    使用UCD3138开发数字电源模块,研发工作已经结束,如何防止烧入程序被复制,在公开资料上没有找到方法,请多多指教,多谢!!!!!!

  • UCD3138_FW_SDK: BidirectionDCDCFirmware-1.2 UCD3138 编译问题

    Part Number: UCD3138

    CCS12 编译 BidirectionDCDCFirmware-1.2 UCD3138出现下列问题,请帮忙解决。谢谢!

    "../Dev/Linker Files/cyclone.cmd", line 97: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that…

  • UCD3138: dpwm_xA比dpwm_xB的脉宽小一点

    Part Number: UCD3138

    我发现这个dpwm在0A和0B的输出上有差异,一样的占空比,为啥总是A比B的脉宽小一点呢?

  • UCD3138: UCD3138的DPWM谐振模式无输出问题

    Part Number: UCD3138

    在经过学习LAB1-4的代码学习之后,已经可以对定频变占空比的DPWM波形进行配置。

    目前想从LAB3的基础上改为开环调频代码吗,通过CPU_sample的值更改输出DPWM的频率,

    但是通过代码发现当DPWM的模式选择为谐振模式时,没有PWM输出;当选择为普通模式时,有PWM输出。

    请问配置谐振模式时,还需要注意哪些寄存器?

    Fullscreen
    1
    //###########################################################################…
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

  • UCD3138: UCD3138例程

    Part Number: UCD3138

    请问哪里可以下载UCD3138输出PWM波以及进行AD采样的例程呢

  • UCD3138A: JTAG仿真异常

    Part Number: UCD3138A
    Other Parts Discussed in Thread: UCD3138

    XDS100V3连接UCD3138A,CCS12.0进行仿真,有时会跑飞。如下图显示Break at address "0xffffffef" with no debug information available, or outside of program code.。但使用GUI将程序下载到3138A中未出现跑飞现象。

  • UCD3138: downloaded the firmware ,but it failed to compile

    Part Number: UCD3138

    I bought an evaluation board of ucd3138evm-150, but I downloaded the firmware program of LLC to CCS, but it failed to compile

    The error is as follows:

    "C:/Users/22326/Desktop/xinjian/Firmware/Device/UCD3138/Linker/cyclone.cmd…

  • UCD3138: pmbus addr

    Part Number: UCD3138

    根据链接https://www.ti.com/tool/FUSION_DIGITAL_POWER_DESIGNER中的c#demo进行二次开发时,没办法扫描到设备的addr 这边用了usb interface adapter 2006与电脑连接 刚启动demo时 会显示扫描到了一个adapter

  • UCD3138PFCEVM-026: UCD3138PFCEVM-026中控制器由UCD改为DSP28335后,电路测试出现的问题

    Part Number: UCD3138PFCEVM-026
    Other Parts Discussed in Thread: UCD3138

    你好,我这边主电路根据UCD3138PFCEVM-026的电路拓扑结构改变而来,去掉了EMI滤波电路,并将采样电路中的采样比值更改了,控制器由UCD3138改为DSP28335进行PFC双环PI控制。目前进行单相Boost PFC进行测试,参数:低压测试时输入20VAC,设定输出50VDC,负载100欧,开关频率为100kHz的双环程序。采样比例:输入电…

  • UCD3138128: Random phase between DPWM modules during resonant mode

    Part Number: UCD3138128
    Other Parts Discussed in Thread: UCD3138

    1. When DPWM was in resonant mode, Phase-trigger register was not taken effect. For example,during DPWM0 and DPWM1  resonant mode, if Dpwm1Regs.DPWMCTRL0.bit.MSYNC_SLAVE_EN = 1; the phase…

1 2 3 4 5 »