我用UCD9222+UCD7242产生C6670的CVDD和VCC1V0,原理图为
板子上电后DSP烧了,取下DSP后测得
CVDD与VCC1V0电压抓取如下图
CVDD电源细节如下图
CVDD这样的电压纹波会烧毁C6670吗???怎样降低这个纹波?加大后级电感值?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
上图哪一个是CVDD?哪一个是CVDD1?
纹波在DSP测不能超过5%,你这个波形像是9222输出错误,建议到电源板块问问。
第一张图中,黄色是CVDD,蓝色是CVDD1
第二张图是CVDD的结果,纹波确实有点大。纹波出现的频率是UCD9222输出的PWM波的频率,即799KHz。
现在我们的问题是:C6670焊接上去后,在上电前测CVDD引脚及CVDD1引脚对地电阻,都是0.2 Ohm左右。
后来怀疑芯片有问题,在E2E上发帖如下
http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/484532/1751307#1751307
我们买到的芯片是C6670,lot trace是“YB20-33V7ZK9”,TI员工在此帖跟贴说这个批次好像确实是无效的,需要我做verification process
但是必须提供采购商的名称、二维码、shipping材料,而我们是从中发小柜台买的,这些材料都没法提供,所以没法做verification process
不知道中国区的TI官方能否查询C6670的批次“YB20-33V7ZK9”,谢谢!