This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

(starterware)AM335X的GPIO0_19可不可以做IO中断



如题,在starterware中的gpioCardDetect例程中:

将原来的SD卡的CD线(SK中的GPIO0_6)更改为GPIO0_19,结果无法进入中断。

1.将GPIO_PMUX_OFFADDR_VALUE(0, 6, PAD_FS_RXE_PU_PUPDE(7));

   改为GPIO_PMUX_OFFADDR_VALUE(1, 16, PAD_FS_RXD_PD_PUPDE(7));

2.#define GPIO_CD_PIN_NUM               (6u)

改为#define GPIO_CD_PIN_NUM               (19u)

问题:

1.为什么我在控制GPIO0_19 高低电平的时候无法进入中断?

2.是不是GPIO0_19不能配置成IO中断啊?

3.想把GPIO0_19配置成中断,应该怎么操作呢?