This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM648视频输出图像差,求助啊

Other Parts Discussed in Thread: TVP5154

前端是TVP5154,后端是SAA7105,采集和显示代码如下:

    /* loop forever performing video capture and display */
    while (status == 0) {

       /* grab a fresh video input frame */
       if(IOM_COMPLETED != FVID_exchange(capChan, &frameBuffPtr))
       {     return;
       } 
       /* display the video frame */
       if(IOM_COMPLETED != FVID_exchange(disChan, &frameBuffPtr)) ---------------------------在此处设置断点
       {
     return;
       } 
    } 

设置断点后,根据frameBuffPtr的数据,在CCS中用view->graph->image画图,图片如下:

继续执行后,最终在屏幕上图像为:

参数设置都是按照TI的例程来的,如下:

#if (CFG_VIDEO_MODE == MODE_PAL)

/* Vport Capture driver configuration.Using embedded sync */
static VPORTCAP_Params vCapParamsChan = CAP_PARAMS_CHAN_BT656_DEFAULT(PAL);

/* TVP5154 EDC driver configuration.Using embedded sync and Composite Analog Channel A for all 8 decoders */
static TVP5154_ConfParams vCapParamsDecoder
                   = CAP_PARAMS_TVP5154_EMBEDDED_DEFAULT(PAL, COMPOSITE_A);

/* Vport Display driver configuration.Using embedded sync */
static VPORTDIS_Params vDisParamsChan = DIS_PARAMS_CHAN_BT656_DEFAULT(PAL);

/* SAA7105 EDC driver configuration.Using Svideo Analog output */
static SAA7105_ConfParams vDisParamsEncoder = DIS_PARAMS_SAA7105_SDTV_EMBEDDED_DEFAULT(PAL720, COMPOSITE);
#endif

SAA7105周边硬件电路基本没啥问题,求高手指导~~~~~~~~~~~~~~~~~~~~~~

  • Pu Jun,

    TI DM648 EVM对于SAA7105的使用如下,是做了图像的缩放的。请问在你的硬件上SAA7105是直接和VP口连的对么?如果是,SAA7105的相关配置是否有做调整?

    http://focus.ti.com/en/pdfs/dsp/dm648evm_trg.pdf

    27.Standard-definition video encoder
    Philips SAA7105H. The SAA7105H is an advanced video encoder that converts 1280 × 1024 resolution digital video data to PAL (50 Hz) or NTSC (60 Hz) video signals. See “2.2.3 Standard-definition video encoder” for details.

  • 硬件上648的输出口VP1是直接与SAA7105相连的.SAA7105的配置没有做过调整。不知道如何进行调整,请求指导,谢谢

  • Pu Jun,

    请阅读一下SAA7105的相关文档,看看当前配置和实际的应用场景是否一致,包括缩放配置,输入是内嵌同步还是外同步等。